Browse FAQs

How much extra space is there to the front and rear of the internal rack posts on the NetShelter CX when the rails are at their furthest positions?

Published date: 08 April 2019

Issue:
Customers need to know how much room there is in the NetShelter CX beyond the rails.

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Customers want to avoid interference with the front door and rear fan units.
 
Resolution: 
Forward of the front rack posts = 100mm / 4”
Rearward of the rear rack posts = 60mm / 2” (Except, where fan modules intrude there is no usable extra space)
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.