Browse FAQs

Can the NetShelter CX integral PDU be replaced, or can another be added if a dual power input is required for redundancy? Which PDU comes in the CX?

Published date: 31 May 2019

Issue:
Need an additional or replacement PDU in the NetShelter CX.

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Additional PDU or replacement necessary
 
Resolution:
Yes, the PDU can be replaced or others can be added.
The original PDU included with the cabinet is the APC part number AP9568 for EMEA cabinets (50Hz), and AP9567 for  NEMA cabinets (60Hz).
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.