Browse FAQs

What is the Active Flow Control of an EcoAisle System and what Cooling System are compatible.

Published date: 03 January 2017

Issue:
What is the Active Flow Control of an EcoAisle System and what Cooling System are compatible. 

Product line: EcoAisle 

Environment:  
Only ACRC100, EcoBreeze, ACRC301S, ACRC301H, ACRC500

Cause:  
Install 

Resolution:  

•         Active Flow Control

-          The active flow controller was designed for various mounting methods in the door header, in a duct or mounted in a U space of the rack.

-          The active flow controller monitors the airflow balance between the cooling system and the IT equipment.  It senses the airflow in the contained aisle and sends a control signal to the cooling equipment to vary the fan speed to match the airflow that the server is producing.

-          The controller has 3 LED rings that will change colors based on differing airflows.  If the cooling unit is providing excess airflow the light color will change to blue.  If the cooling unit is not providing enough airflow the light color will change to red.  If the cooling unit is providing  the right amount of airflow the light color will change to Green.

-          This option is only available with the ACRC100 series as well as the EcoBreeze unit at the time of release.  The other products will have the firmware modified to allow compatibility at a future date. 

 

Controller Monitors Airflow Balance Between Cooling System and IT Equipment
Air Balance Control Device - Front.tif  

Cooling Status

Green – optimal

Red – Insufficient Airflow

Blue – Excess Airflow

 

                                                      Controller Mounts above EcoAisle Safe Slide Door

 

 

Cooling Status

Green – optimal

Red – Insufficient Airflow

Blue – Excess Airflow

 

 

 

 

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.