Browse FAQs

How do I update the “Date of last Battery Replacement” seen in NMC card GUI?

Published date: 30 July 2018

Issue:
How do I update the “Date of last Battery Replacement” seen in NMC card GUI?
 
Product line:

Smart-UPS VT, Galaxy 3500, Symmetra PX1
 
Environment:
All models, all serial numbers
 
Cause:
The system does not automatically update battery age / replacement information, it must be manually changed whenever all of the batteries are replaced.
 
Resolution:

Log into the NMC web interface click on the UPS tab then under the Configuration section is the option for General, select General and you will see the options for “last battery replacement”
 

 
And
 

 
 Update when all batteries have been replaced.
 Note, This only applies to units running FW 5x or lower
 
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.