Browse FAQs

ISX-PDU; How to wire and configure the user input and output contacts via the User Connection plate

Published date: 13 August 2013

 
 
Issue:
How to wire and configure the user input and output contacts via the PDU User Connection plate
 
Product line:
ISX-PDU
 
Environment:
All models, all serial numbers
 
Cause:
User Connections to the PDU Monitoring Unit (Brains) is done thru the User Connection plate. User connections may be for EPO interface, input and output contacts.
 
Resolution:
Please refer to attached PDF files detailing the User Connection plate and how to configure the PDU user input and output contacts via the PDU PowerView display contacts screen.
 
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.