Browse FAQs

Presets overwritten when more than one NetBotz appliance monitors a Pelco Camera

Published date: 20 March 2015

Issue:

When more than one NetBotz appliance monitors the same Pelco camera, Pelco camera presets can be overwritten.

Product Line:

NetBotz, Pelco

Environment:

NetBotz software Interfaces

Cause:

The NetBotz appliance sets presets using the default pointer on the camera, “Preset 1”.

Users are allowed to discover the same Pelco camera on more than one NetBotz appliance. No warning message is displayed.

Resolution:

Users should not discover the same Pelco camera on more than one NetBotz appliance.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.