Browse FAQs

What are the length of the power cords of an ACSC

Published date: 14 June 2019

Issue:
What are the length of the power cords of an ACSC.                        

Product line:
ACSC100, ACSC103. 

Environment:
All Product models, all serial numbers. 

Cause:

Resolution:

ACSC Power cord lengths

          60 Hz unit – 5.5 Feet (1.7 m)

          50 Hz unit – 12 Feet (3.6 m)

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.