Browse FAQs

Windows Server 2008 R2 Server Core/ Windows HyperV Server 2008 R2: High CPU Usage for Java.exe

Published date: 15 May 2018

Issue:
Windows Server 2008 R2 Server Core/ Windows HyperV Server 2008 R2: High CPU Usage for Java.exe

Product Line:
PowerChute Network Shutdown
PowerChute Business Edition

Environment:
Windows Server 2008 R2 Server Core/ Windows HyperV Server 2008 R2

Cause:
This is a known Microsoft issue specific to Windows 2008 Server Core R2 and Windows HyperV Server 2008 R2 - see http://support.microsoft.com/kb/978309.

Solution:

If you experience this issue you should stop the PowerChute service, install the Microsoft hotfix for KB978309 and re-start the machine.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.