Browse FAQs

PowerChute Personal Edition 3.0 un-installation hangs while re-enabling hibernation on Windows.

Published date: 23 July 2018

Issue:
PowerChute Personal Edition 3.0 un-installation hangs while re-enabling hibernation on Windows.

Product Line:
PowerChute Personal Edition 3.0

Environment:
All supported Windows OS

Cause:
If the text on your screen says re-enabling hibernation, this is happening because the USB port cannot be detected by Windows Device Manager. After the system restart, the USB port will work fine.

Solution:

Restart your PC and then try to uninstall PowerChute Personal Edition 3.0.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.