Browse FAQs

Error When Attempting a Runtime Calibration in PowerChute Business Edition

Published date: 24 October 2018

Issue:
Error When Attempting a Runtime Calibration in PowerChute Business Edition

Product Line:
PowerChute Business Edition

Environment:
All supported OS

Cause:
1) The battery has less than 100% charge:
2) The load on the UPS is 10% or less:

Resolution:
Two conditions need to be met in order to perform a calibration:

1) The battery charge needs to be at 100%,
2) The load on the UPS needs to be greater than 10% of the battery capacity


 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.