Browse FAQs

How to Brain Dead a Back-UPS unit. (Full UPS Logic Reset)

Published date: 11 July 2018

Issue:

To brain dead a Back-ups is to purge the charge in the brain of the UPS.

Product Line:

Back-UPS, Back-UPS Pro

Environment:

All serial numbers.

Cause:

Troubleshooting procedure often prescribed to clear some faults or unwanted behaviors.

Resolution:

To do this, follow the below procedure;
 

1: Disconnect any attached load.

2: Unplug the UPS from the wall socket.

3: Disconnect the UPS' internal battery.

4: Push and hold the ""On"" button on the UPS for 5 seconds

5: Reconnect internal battery.

6: Plug UPS in to known good power source.

7: Turn UPS on.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.