Browse FAQs

EMI/RFI Filtering of the S-Type, AV Power Conditioners w/Battery Backup.

Published date: 11 June 2019

Issue:

What type of EMI/RFI filtering does the S-Type, AV Power Conditioners w/Battery Backup have?

Product Line:

S10 / S15
S10BLK / S15BLK / S20BLK

Environment:

N/A

Cause / Resolution:

The S-Type, AV Power Conditioners w/Battery Backup provide application-specific EMI/RFI isolated filter banks, which help to improve audio and video signaling.

• Filter Banks improve sound and video for systems affected by electro-magnetic and radio frequency interference on the AC utility line.

• Banks are isolated to prevent device noise from polluting other connected components.

• Each filter bank is specifically tuned to filter noise for a particular class of component. Specific filter banks are provided for Digital, Analog and High-Current components.

• Unlike filters from many competitors, APC’s High-Current filter also protects high-powered amplifiers and subwoofers, without compromising their ability to draw high currents during periods of peak sound output. It is not necessary to plug an amplifier into a separate wall outlet.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.