Browse FAQs

What's the difference between shipping load, dynamic load and static load? How are these ratings calculated?

Published date: 24 January 2019

Issue:
Customers need to know the difference between shipping load, dynamic load and static load ratings, and how they are calculated.

Product Line:
NetShelter SX
 
Environment:
All versions and serial ranges.
 
Cause:
Customers need to make sure the they do not exceed the load capacity of the cabinet during installation, travel or operation. Some may be wondering if they can safely exceed these ratings or recalculate them.
 
Resolution:

Please see attachment.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.