Browse FAQs

Does the AR2144BLK or AR2145BLK NetShelter VX Seismic have leveling feet or castors available as an accessory?

Published date: 19 August 2019

Issue:
A customer may ask if castors are an accessory for our NetShelter VX cabinet.

Product Line:
NetShelter VX 
 
Environment:
All versions and serial ranges.
 
Cause:
Castors can be used to move the cabinet much eaqsier.  
 
Resolution :

The NetShelter VX cabinets do not offer castors as an accessory. These cabinets are approved for NEBS GR-63-CORE seismic installation, which does not include the use of castors.
Also see attached document.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.