Browse FAQs

Is there a roof available for the AR3100 which is solid and does not have open cable access holes?

Published date: 29 November 2018

Issue:
Customers may need for a solid roof on their cabinets.

Product Line:
NetShelter SX
 
Environment:
All versions and serial ranges.
 
Cause:
A more secure roof may be required for installations such as PCI.
 
Resolution:
The WAR7210 can be used where high security is required. It is compatible with the following models: AR3100, AR3104, AR3105, AR3200 and AR3107.
For more information and a photo please see the attached file.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.