Browse FAQs

Will the NetShelter SX leveling feet support the full weight of the cabinet and its contents?

Published date: 12 June 2019

Issue:
Can the full weight of the NetShelter cabinet rest on the leveling feet?
 
Product Line:
NetShelter SX
 
Environment:
All versions and serial ranges.
 
Cause:
Cabinets are leveled using the leveling feet so  they need to bear the full weight of the cabinet and it's contents. (static load rating)
 
Resolution:
Yes, the leveling feet can support the cabinet up to the rated static load rating of the cabinet.  
FAQ FA158656 also contains information regarding shipping load, dynamic load and static load ratings.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.