Browse FAQs

Are there spare or replacement keys available for the NetShelter SX, SV or VX cabinets?

Published date: 30 May 2018

Issue:
Customers require spare keys for their cabinets?
 
Product Line:
NetShelter SX, NetShelter SV, NetShelter VX
 
Environment: 
All models and serial ranges.  
 
Cause:
Keys can be lost, or extras may be needed.
 
Resolution : Yes, a spare key can be purchased using Part number W870-8135. This is a single spare key which works on the NetShelter SX, SV and VX doors and side panels.
It also works on the NetShelter WX models AR106, AR109 and AR112.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.