Browse FAQs

Alarms in InfraStruXure Central and StruxureWare DCEl show up with a period for a decimal separator even if a different regional setting is applied.

Published date: 29 June 2018

Issue:
Alarms in InfraStruXure Central and StruxureWare Central show up with a period for a decimal separator even if a different regional setting is applied.

Product Line:
InfraStruXure Central, StruxureWare Data Center Expert.

Environment:
All versions

Cause:
Not Provided

Resolution:
This issue appears only in the alarm view in the InfraStruXure/StruxureWare Central client interface. External sources such as an e-mail caused by the alert will have the proper separator based on the chosen region in Central. Data in reports should also have the proper separator. This is a cosmetic issue only.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.