Browse FAQs

PTZ or motion detection functions on an existing Pelco camera no longer work through NetBotz appliance after upgrade to 3.3

Published date: 14 August 2013

Issue:

PTZ or motion detection functions on an existing Pelco camera no longer work through NetBotz appliance after upgrade to 3.3

Product Line:

NetBotz

Environment:

NetBotz 3.3. upgrade

Cause / Resolution:

If after upgrading from 3.2.x to 3.3.x, the PTZ or motion detection functions on an existing Pelco camera no longer work the camera has to be removed and re-added and shared. Possible cause is that the user upgraded to 3.3.x Advanced View but did not upgrade to 3.3.x on the appliance and then added the camera. The user should upgrade both Advanced View and the appliance before adding the Pelco camera. An existing camera added with matching software and firmware will not have this issue.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.