Browse FAQs

SSH server running after restored configuration of InfraStruXure Central

Published date: 14 November 2013

Issue:

SSH server running after restored configuration of InfraStruXure Central

Product Line:

InfraStruxure Central

Environment:

InfraStruxure Central
StruxureWare Central
StruxureWare Data Center Expert.

Cause:

If SSH is turned on, it will be turned off after the configuration is restored as this is the default setting.

Resolution:

This issue was found in ISXC 5.1.1 and the only current resolution is to manually reconfigure SSH settings.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.