Browse FAQs

Only Alerts Associated with Default Alert Profile are Posted if Netbotz device is in post only mode.

Published date: 14 November 2013

Issue:

Only Alerts Associated with Default Alert Profile are Posted if Netbotz device is in post only mode

Product Line:

NetBotz

Environment:

NetBotz post only mode

Cause:

If your appliance is set to InfraStruXure Central Post-Only Mode (Tools > Advanced > InfraStruXure Central Post-only Mode), alert notifications that occur as a result of alert actions associated with the Default Alert Profile are posted automatically. Alert notifications associated with any other alert profiles are not posted to InfraStruXure Central.

Resolution:

If you use Post-Only mode, use only the Default Alert Profile. If this is not an option, configure the Data Collection and Monitoring settings for post-only appliances for your InfraStruXure Central appliance to shorter intervals so that alert conditions are more likely to be detected.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.