Browse FAQs

Downloading the MIB file for version 3 Netbotz.

Published date: 13 February 2018

Issue:

Downloading the MIB file for version 3 Netbotz.

Product Line:

NetBotz

Environment:

NetBotz version 3 MIB

Cause:

Obtaining the NetBotz version 3 SNMP MIB file

Resolution:

The SNMP MIB for NetBotz Appliances can be downloaded from the NetBotz Appliance itself by accessing the following URL:

http://ip_address_of_appliance/netbotz300.mib

In versions of Botzware after 3.1.2, the link will be more similar to the version 2 URL

V2:
http://ip_address_of_appliance/netbotzv2.mib

V3
http://ip_address_of_appliance/netbotzv3.mib

The latest MIB should also be available on the APC software downloads page at:
http://www.apcc.com/tools/download
Sort the selection by firmware upgrades - MIB

It should also be available on the product page for individual NetBotz appliances under the documentation tab.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.