Browse FAQs

Updating Firmware to APC devices from InfraStruXure Central fails when updating 350 or more nodes.

Published date: 18 December 2013

Issue:

Updating Firmware to APC devices from InfraStruXure Central fails when updating 350 or more nodes.

Product Line:

InfraStruxure Central

Environment:

InfraStruxure Central any version
APC SNMP devices and firmware updates.

Cause:

When updating the firmware APC devices from InfraStruXure Central, you can select specific nodes to upgrade.

Resolution:

APC recommends selecting a lower amount of devices to update such as 100 nodes at a time.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.