Browse FAQs

Is the AP9361 (Netbotz Rack Access PX - HID) compatible with VX racks?

Published date: 13 March 2018

Issue:

Is the AP9361 (Netbotz Rack Access PX - HID) compatible with VX racks.

Product Line:

NetBotz

Environment:

NetBotz rack access

Cause:

Compatibility

Resolution:

No. The AP9361 (Netbotz Rack Access PX - HID) is not compatible with VX racks. The AP9361 is only compatible with the SX and SV racks. The NetBotz rack access pod (NBPD0171) uses the same handle as the AP9361 and it too is incompatible with the VX racks.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.