Browse FAQs

Display of hostname on ISX Central/Netbotz Central map view

Published date: 22 November 2013

Issue:

Display of hostname on InfraStruxure Central/Netbotz Central map view

Product Line:

InfraStruxure Central/Netbotz Central

Environment:

Any version

Cause:

Hostname information

Resolution:

Hostname can be set as the tag but the hostname and IP address need to be resolvable in the local DNS server. Once that is done, go to the Central's tools/preferences menu and click on general and change display device to read hostname


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.