Browse FAQs

DIN Connector Pin Outs For the Netbotz Appliances

Published date: 19 December 2014

Issue:
DIN Connector Pin Outs For the Netbotz Appliances

Product Line:
NetBotz

Environment:
NetBotz version 1 and 2 cables

Cause:
Pin-out specifications.

Resolution:
DIN Connector Pin Outs

-NetBotz does not release the pin outs for the DIN connectors for any NetBotz Appliances.

-To address this issue, NetBotz sells a standard dry contact cable that is our DIN connector one end and two bare dry contact style wires on the other.

-This cable is provided to allow customers to attach our NetBotz Appliances to any dry contact type connection without having to have the DIN connector pin outs.




 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.