Browse FAQs

Details Returned from DMTF Devices via Advanced Device Crawlers

Published date: 26 May 2015

Issue:

Details Returned from DMTF Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for DMTF systems assuming the DMTF DDF (Device Definition File) is installed on the NetBotz appliance and the DMTF system is SNMP enabled. Please note that not all information listed below is available on all DMTF models.

Resolution:

 
  • Status
  • Power Supply Status
  • System Thermal Status
  • UPS Battery Status
  • Seconds on battery
  • Battery Run Time Remaining
  • Remaining Battery Capacity
  • Battery Voltage
  • Battery Current

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.