Browse FAQs

Details Returned from Alcatel Devices via Advanced Device Crawlers

Published date: 26 May 2015

Issue:

Details Returned from Alcatel Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Alcatel systems assuming the Alcatel DDF (Device Definition File) is installed on the NetBotz appliance and the Alcatel device is SNMP enabled. Please note that not all information listed below is available on all Alcatel models.

Resolution:
 
  • Description
  • Power Supply
  • Primary MPM Temp Sensor
  • Secondary MPM Temp Sensor
  • Fan Tray

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.