Browse FAQs

Amp detector Readings Fluctuate Showing .1 or .2 Amps in Netbotz

Published date: 08 January 2014

Issue:

Amp detector Readings Fluctuate Showing .1 or .2 Amps in Netbotz with no load

Product Line:

NetBotz

Environment:

Version 1 and 2 amp detectors

Cause:

Amp Detector is a passive device. The .1 or .2 readings are interference readings.

Resolution:

To get a proper reading a load must be connected to it and be pulling power


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.