Browse FAQs

Standard Lens Specifications for the WallBotz 500 & version 1 Camera Pod 120

Published date: 30 January 2014

Issue:

Standard Lens Specifications for the WallBotz 500 & version 1 Camera Pod 120

Product Line:

NetBotz

Environment:

NetBotz camera pod NBPD0121

Cause:

Lens specifications.

Resolution:

Lens Specifications for the standard lens on the WallBotz 500 / Camera Pod 120:

Manufacturer: Marshall Electronics

Model: V-4508

Size: 1/2 inch format

Focal Length: 8mm
Note: The focal length is the distance between the lens and the imager.

F-Stop: 1.3
Note: The f-stop affects depth of field, or how much is in focus in front of and behind the subject.

Field of View (horizontal x vertical in degrees): 40x28

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.