Browse FAQs

Camera Specifications for NetBotz 500 & Camera Pod 120

Published date: 20 January 2014

Issue:

Camera Specifications for NetBotz 500 & Camera Pod 120

Product Line:

NetBotz

Environment:

NetBotz 500 and NBPD0121

Cause:

Camera specifications.

Resolution:

WallBotz 500 / Camera Pod 120 Camera Specifications

Resolution Maximum Resolution Frame Picture Size
160x120 30 frames per second 1.2KB to 5KB
320x240 30 frames per second 8KB to 13KB
640x480 30 frames per second 30KB to 51KB
800x600 10 frames per second 50KB to 73KB
1024x768 10 frames per second 70KB to 114KB
1280x1024 10 frames per second 100KB to 175KB

 



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.