Browse FAQs

How do I obtain Wireless Network Status Information for Version 2 Appliances

Published date: 20 January 2014

Issue:

Wireless Network Status Information for Version 2 Appliances

Product Line:

NetBotz

Environment:

NetBotz version 2

Cause:

Obtaining status of attached wireless cards.

Resolution:

The following URL will display the 802.11 network status information when an 802.11 a/b/g card is installed in a NetBotz 420 or 500.

http://<bot_ip>/wireless.status



Where <bot_ip> is the IP address or hostname of the appliance.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.