Browse FAQs

Can I install battery modules in the power module bays with my Symmetra RM 2-6kVA UPS?

Published date: 14 January 2014



Yes.  The Symmetra RM 2-6 kVA system will accept battery modules (part no. SYBT2) in the bottom three power module bays to provide additional runtime if the bays are not being occupied by power modules.  The L1 bay is the only bay that cannot accept a battery module. No other single phase Symmetra is capable of this.




Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.