Browse FAQs

Verification of Matrix-UPS input voltage configuration

Published date: 03 June 2014


Issue

How do I verify the position of the input voltage selector wire on a Matrix?


Product Line

Matrix UPS


Environment

All serial ranges


Cause

The Matrix must be configured for a 208 or a 240 environment.  The instructions in this document help the user determine the position of this selector wire without physically checking.


Resolution

The North American Matrix-UPS 3000 and 5000 units are wired at the factory for a 208 Vac input. If the Matrix-UPS is to be used in a 240 Vac environment, the Input Voltage Select Wire must be physically moved. This document describes a procedure that can be used to verify the setting.

If the unit is in place and operating, follow these steps to verify proper installation:

1 ) Go to the front display of the Matrix-UPS and access the UPS Status menu, then scroll through to check the input line voltage with the sub-menu Line = xxx.x Vac in some cases this value may not be near either 208 Vac or 240 Vac due to high or low input line.

2 ) Next, go to the menu UPS Diagnostics menu and scroll to the sub-menu UPS FW rev: xxx; on this sub-menu screen will be the revision of the Electronic Unit's UPS control microprocessor. The third x will either be a letter I or a letter M.

If there is a letter M, the Matrix-UPS Input Voltage Select Wire is attached to the 208V tap; therefore, the input voltage should be approximately 208V. If there is a letter I, the Matrix-UPS Input Voltage Select Wire is attached to the 240V tap; therefore, the input voltage should be approximately 240V.

OR

Use the UPS Setup menu. It has a sub-menu named OutVReport. If the report is set to 'Auto,' then the Output submenu under the UPS Status menu will reflect the actual output voltage from either the L6-30R or the L14-30R.  If UPS FW rev has the letter M, then the Output submenu reflects the L6-30. If UPS FW rev has the letter I, then the Output submenu reflects the L14-30.

If you are inputting 240 Vac to the Matrix-UPS, but did not change the Input Voltage Select Wire to that setting, the letter M will show under UPS FW rev: xxx; this should be a letter I. Reference the Matrix-UPS manual in order move the Input Voltage Select Wire. If this is not done, the Matrix-UPS will either stay in bypass mode or constantly change its transformer taps. Other Select Wire failures may also be displayed on the front LCD display.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.