Browse FAQs

Single Phase Symmetra SmartSlot Device Installation

Published date: 15 October 2013


Issue:


In order to ensure proper operation, SmartSlot cards must be installed in a certain, specific order according to precedence


Product Line:

Single Phase Symmetra and smart-slot accessories.

Note: Only SmartSlot accessories with revision K or later can be integrated with the Symmetra.


Resolution:

When placing multiple SmartSlot accessories in the Symmetra expansion slots, great care must be taken so the correct ordering of the accessories observed. A SmartSlot device with higher priority must be placed in the SmartSlot labeled with the higher number. Refer to the following table for details.

  PART NUMBER PRIORITY POSITION
Network Management Card

AP9606
AP9617
AP9618
AP9619
AP9630/30CH
AP9631/31CH

Highest Highest-numbered slot
Call-UPS II Out of Band Management SmartSlot Card AP9608 Second highest Second-highest-numbered slot (highest if no network management card is present)
Dry Contact I/O SmartSlot Card AP9610
AP9613
Medium Any slot numbered lower than a network management card, Call-UPS II; any slot higher than Measure-UPS
Interface Expander SmartSlot Card AP9607 Medium Any slot numbered lower than a network management card, Call-UPS II; any slot higher than Measure-UPS
Measure-UPS SmartSlot Card AP9612T
AP9612TH
Lowest Lowest-numbered slot



The following graphic is an example of how to install multiple SmartSlot devices in the Symmetra Power Array. Please note the numbering shown in the figure. The network management card is installed in slot #4, Call-UPS II in #3, Interface Expander in #2, and Measure- UPS in #1.




The following graphic is an example of how to install multiple SmartSlot devices in the Symmetra RM and Symmetra LX.  The network management card is installed in slot #2 and Call-UPS II is installed in slot #1.


 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.