Browse FAQs

ISX Central | Enabling or disabling the private LAN will cause a new self signed SSL certificate to be generated.

Published date: 07 September 2018

Issue:
Enabling or disabling ISX Central Private LAN will cause the server to generate a new self signed SSL certificate

Product Line:
InfraStruxure Central (ISXC)

Environment:
InfraStruxure Central (Prior to 6.2)

Cause:
When working with SSL certs, you will need to re-add the cert if you enable or disable DHCP on the private LAN or if you change IP information on the private LAN. This is a known issue.

Resolution:

This issue was resolved in InfraStruxure Central 6.2
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.