Browse FAQs

On the RP Chilled Water the top piping connections have one pipe for the return plumbed to the top, but no supply pipe connection, is this normal?

Published date: 10 January 2018

Issue:
On the RP Chilled Water the top piping connections have one pipe for the return plumbed to the top, but no supply pipe connection, is this normal?
 
Product line:
ACRP50x
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
Yes this is normal. In the crating of each unit will be two long extension pipes that is field installed and insulated. If you need more clearance, it is suggested to use the flex pipe kit.







 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.