Browse FAQs

Can your InRow Cooling Auto-Start after a Power Failure

Published date: 24 January 2018

Issue:
Can your InRow Cooling Auto-Start after a Power Failure
 
Product line:
InRow
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
The InRow RC, RD, RP and SC will start automatically if the power is restored after a power failure. The unit will go to its last known state, ie if the unit was in standby, the unit would return to standby, or if the unit is on, the unit would return to the on state.

It is also possible to configure a Start up Delay of 0 to 999 seconds.

That can be done from:
  1. The Display: Configure Unit>General> Startup Delay
  2. The Network Management Card Interface: Unit>Unit Configuration> Startup Delay

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.