Browse FAQs

FM Expansion Module PCIOM I/O mapping for System ON

Published date: 16 May 2019

Issue: FM PICOM I/O Mapping for System On
 
Product line: FM
 
Environment: Data Center Cooling
 
Cause:
 
Resolution:
FM Expansion I/O for System ON

Output #2 of the Expansion Module (EM) PCIOM is always mapped to System On. You can wire this to an input on the Main Module's (MM) PCIOM, then map that input to the output that you have the MM's System On mapped to. This should assert that output if either the MM or the EM is shut off.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.