Browse FAQs

InRow Firmware Upgrade via multiple NMC Cards(ACRC, ACRP , ACSC, ACRD)

Published date: 24 January 2018

Issue:
InRow Gen1 Firmware Upgrade via multiple NMC Cards(ACRC, ACRP , ACSC, ACRD)

Product line:
InRow Cooling

Environment:
Data Center Cooling

Cause:

Resolution:
See the attached document, which will explain how to install and execute an NMC firmware upgrade for multiple units that are using the same firmware. For example, if you have 102 ACRC101, or a total of 50 ACRP100s and ACRD500s. See list of units below that use the same firmware.

ACRC
ACRC100, ACRC101, ACRC103

ACSC
ACSC100, ACSC101

ACRD
ACRD100, ACRD101, ACRD200, ACRD201

ACRP (600mm units)
ACRP100, ACRP101, ACRP102, ACRP500, ACRP501, ACRP502, ACRC500, ACRC501, ACRC502, ACRD500, ACRD501, ACRD502


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.