Browse FAQs

InRow Entering Fluid Temp threshold is not alarming

Published date: 24 January 2018

Issue:
InRow Entering Fluid Temp threshold is not alarming 
 
Product line:
InRow
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
In the newest firmware ACRC 372 and higher the entering fluid temp alarm threshold violation will not be reported unless two conditions are met. The unit has a >=40% valve position opening, and the entering temperature is above the threshold.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.