Browse FAQs

PowerChute Network Shutdown 2.2.4 and 4.5G and 5G Smart UPS Behavior

Published date: 21 March 2014


Issue

When using Powerchute Network Shutdown 2.2.4 and Network Management Card 2 UPS application firmware revision apc_hw05_sumx_v5.0.3 (SFSUMX503), selecting the option to turn off the UPS via PowerChute Network Shutdown is supported for only the 'On Battery' and 'Low Battery' UPS events on certain Smart-UPS models.

Should a user attempt to use the turn off UPS functionality via PowerChute Network Shutdown for other events, the UPS will not turn off. Furthermore, should the user restart the server running PowerChute Network Shutdown, the server will shutdown immediately.



Product Line
 
 

  • Smart-UPS Models:
    • SMT750
    • SMT1000
    • SMT1500
    • SMT2200
    • SMT3000
    • SMX750
    • SMX1000
    • SMX1500RM2U
    • SMX1500RM2UNC
    • SMX2000RMLV2U
    • SMX2200RMLV2U
    • SMX3000RMLV2U
    • SMX3000RMLV2UNC
  • UPS Network Management Card 2
    • AP9630
    • AP9631



Environment

  • AP9630/31 sumx application v5.0.3
  • All serial numbers


Cause

This is due to the initial implementation of v5.0.3 sumx application for particular UPS models.



Resolution

It is recommended that users upgrade to SUMX application 5.1.1 or higher to resolve this issue at https://www.apc.com/tools/download.

In order to rectify the server restart/shutdown situation without upgrading, the user must manually turn off the UPS and then turn it back on.




Please note: Any prior version of PowerChute Network Shutdown will not work with the aforementioned UPS models.




Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.