Browse FAQs

Network Management Card - Single Phase Symmetra SNMP Trap #77 details

Published date: 04 June 2019


Issue

Network Management Card - Single Phase Symmetra SNMP Trap #77 details

Product Line
 

  • UPS Network Management Card 1 - AP9617, AP9618, AP9619
 
  • UPS Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH
     


Environment
 
  • All serial numbers
  • All firmware versions
  • SNMPv1 or v3 traps


Cause

SNMP trap # 77 (abnormalCondition) is reserved for specific UPS failures. When trap #77 is sent, it also has a binded subtrap which gives further detail into the nature of the fault. The subtraps are specific to the UPS family type. 


Resolution

Attached is a breakdown for the Symmetra single phase line of UPS (Symmetra RM, Symmetra LX, Symmetra Power Array), which uses the Network Management Card APP called 'sy'.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.