Browse FAQs

What are the main difference between the AP9550, AP9551, AP9553, AP9554, and the AP9555 Rack Power Distribution Units?

Published date: 06 March 2018



The only differences between the units below are as follows:

 

 Model

 Mounting

Input

 Output

 Voltage Input/Output

 Max Amperage Draw

 AP9550

 Horizontal

 L5-20P

 5-15R

 100v-125v

 20A

 AP9551

 Vertical

 L5-20P

 5-15R

 100v-125v

 20A

 AP9553

 Horizontal

 IEC Outlet

 IEC Outlets

 120v-240v

 10A

 AP9554

 Vertical

 IEC Outlet

 IEC Outlets

 120v-240v

 12.8-16A

 AP9555

 Horizontal

 5-20P

 5-15R

 100v-125v

 20A





 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.