Sfoglia le FAQ



Can StruxureWare Data Center Expert be configured to alert for NetBotz 3xx, 4xx, and 5xx devices?
Please note that this is different than the NetBotz Rack Access AP9361, NetBotz 200 , or NetBotz 250 which are monitored using SNMP.
What is the maximum number of rack access cards that can be configured in a version 3 NetBotz appliance for use with the rack access pod 170?
When using StruxureWare Data Center Expert to configure multiple NetBotz appliances, the limit in this system is also 200 cards and again all cards ...
Data Center Operation | Functionality Matrix
Resolution: See attachment for StruxureWare Data Center Operation Functionality Matrix.
Video: How do I register a passcode for NetBotz or StruxureWare?
... key you are redeeming, select either: Data Center Expert Model, NetBotz Model, or SFDCOBase (Data Center Operation ).
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
How to copy files from the StruxureWare Data Center Operation ... StruxureWare Data Center Operation ... StruxureWare Data Center Operation (All Versions) ... Files such as backup and logs can be "downloaded" from the Operation server using SFTP/FTP. In this document, we will be using a free program called WinSCP. You can find this program . Please see the instructions below for a step by step guide for "downloading" files from the server via WinSCP. 1. Open the application
Where can I view community resources and documentation for Data Center Operation?
Product Line StruxureWare Data Center Operation (DCO)
Why does my Rack ATS (AP77XX) lose snmpv1 communication with my StruXureWare device or ISX Manager?
My Rack ATS (AP77XX ... communication with my StruXureWare device, ISX ... ... Only the following Rack Automatic Transfer Switch ... Rack ATS app g2ats v3 ... Rack ATS monitored by ... ... aforementioned Next Generation Rack ATS product firmware ... snmpv1 communication with StruXureWare , ISX Manager ... other SNMP monitoring programs . This issue occurs after an undefined amount of uptime but limiting access control to specific devices seems to help increase the uptime to about 30-45 days for the integrated Network Management Card. ... This has been addressed in Rack ATS Firmware g2ats v3.7.0 and higher.
Data Center Operation | What security vulnerability is this software vulnerable to?
Issue: What security vulnerability is StruxureWare Data Center Operation vulnerable to?


Risultati 1 - 10 di 71

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.