Sfoglia le FAQ



Can I use a NetBotz Camera Pod 160 nbpd0160 / nbpd0160a as a standalone appliance?
Issue: A customer may purchase a solution with the intension of using a NetBotz camera pod 160 on its own.
Newly attached camera pod on a version 3 Netbotz appliance does not show time stamp.
This happens to both the newer camera pod 160 as well as the older version 2 camera pod 120.
"Slave Device Failure" message polling NetBotz device.
... error will occur when polling the register assigned to the door switch on a camera pod 160 if the door switch is not connected.
What kind of microphone can I use on a NetBotz appliance / Camera pod 160?
Issue: What kind of microphone can I use on a NetBotz appliance / Camera pod 160 ?
Data Center Expert | NetBotz 750 camera thumbnail must be manually deleted from surveillance view
When you remove a version 2 or 3 NetBotz appliance with a camera pod 120 or 160 from a DCE server, the camera thumbnail ...
Netbotz | Can a configuration backup be used on another NetBotz appliance?
Due to differences in NetBotz Pod and sensor IDs from one appliance to another, importing a backup from one appliance to another will not ...
NetBotz Camera Pod 165 Firmware Upgrade
Issue: NetBotz Camera Pod 165 Firmware Upgrade Procedure
NetBotz wireless pod data loss if nbpd0180 coordinator is disconnected.
Issue: NetBotz wireless pod data loss if nbpd0180 coordinator is disconnected


Risultati 1 - 10 di 50

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.