How tall is the NetShelter WX with the optional castor kit attached?
Issue: Customers may ask for the total height of the NetShelter WX with the optional castor kit attached.
What is the maximum equipment & cable mounting depth for the NetShelter WX?
Issue: Will deep IT gear fit into the NetShelter WX , and if so, how much clearance will remain for cabling?
Does the NetShelter WX castor kit AR8359 fit onto the ar106, ar109 or AR112.
Issue: There doesn't appear to be a castor kit for the 6U, 9U or 12U NetShelter WX cabinets.
What spare parts are available for my NetShelter SX, VX, WX, AV, SV, Colocation, EP, ES, VS, 2-Post Rack, 4-Post Rack?
Product Line: NetShelter SX, NetShelter VX, NetShelter CX, NetShelter WX , NetShelter SV, NetShelter ES, NetShelter EP, NetShelter VS.
Are NetShelter cabinets PCI Compliant?
Product Line: NetShelter SX, NetShelter CX, NetShelter WX , NetShelter SV
Are NetShelter SX, SV, CX or VX cabinets NEMA rated?
Product Line: NetShelter SX, NetShelter SV, NetShelter CX, NetShelter VX, NetShelter WX