Sfoglia le FAQ



Can a 0U PDU be hung upside down in the NetShelter SX cabinet?
A customer may want to install the 0 U PDU with the power supply cord facing either the top or bottom of the cabinet depending ...
Is there a way to attach 0U PDUs to a NetShelter 2-post rack?
Issue: A customer wants to use a 0 U PDU with a NetShelter 2-post rack.
Can the center dividing section of the NetShelter SX Colocation be removed?
For various reasons, including the want to mount a particular 0 U PDU , customers may wish to remove the center divider of the ...
Can a full height 0U PDU be installed into the NetShelter SX Colocation cabinet?
The NetShelter Colocation cabinet does not support the use of a 0 U PDU .
Differences between ap7xxx and ap7xxxb Series Rack PDU's
Discontinued: Metered AP7851 - RackPDU,Metered, 0 U AP7851
Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
... for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0 U accessory channel.
Choosing the Correct NMC Firmware Upgrade Executable for Your Modular PDU
... PDPM72F-5 U ,PDPM138H-5 U ,PDPM138H-R, 0 g-9354 ... Executable, Modular PDU , Transfer Failed, 0 G-9354A-01, 0 G-9354A
What is the distance between PDU mounting holes on the NetShelter SX accessory rails?
In the 42U cabinet There are 6 sets of PDU mounting holes, all are spread by 7 U (311mm 12.25")
Is there documentation of any NetShelter fitment issues with OEMs like Dell, HP or IBM?
Cause: Some manufacturer's rail kits can be very long or interfere with ports on a PDU .


Risultati 1 - 10 di 50

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.