Sfoglia le FAQ



Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
1 ) You must ... ... beyond the base 25 device nodes and 1 surveillance node) ... After verifying support contracts for the license keys and the server itself, technical support can reset the license key passcodes so that they may be used again to license the virtual server. Technical support will work with the contract administrators to switch the support contracts to the new servers/licenses. ... These changes (at least the NIC addition) should be done prior to the first boot up of the DCE VM. Do not add drive space to the default drive as per fa309639
Data Center Expert | How do hardware and software support contracts work?
... warranty and software support contracts work for StruxureWare ... Software Support Contract software support . ... and any additional device packs must be ... and complete software support in order to ... Software support contracts are required for ... has a default 25 nodes (covered under base software support SKUs) as ... ... not currently require support contracts . Hardware Support Contracts Hardware support must be continuous ... Year 1 ... Out of HW Support ap9470 Factory Factory ... Out of HW Support AP9475 Factory Factory ... Out of HW Support Software Support Contracts Software support can not be ... Support contracts start at the ... date of previous contracts .
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
... Card-enabled device or need to ... Devices with an embedded ... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... Devices with an embedded Network Management Card 1 include (but ... Devices with an embedded ... ... Network Management Card device send email to ... 1 .) Within ... 1 .a) ... ... is recommended you change the From Address Allow 1 -2 minutes ... ... that TCP port 25 is open. ... ISP's block port 25 since it has ... ... X do not support . ... be able to support SSL authentication. ... mail server, changing your From Address
APC Security Advisory - Static Factory Password Vulnerability
... control of these devices . ... server or similar device . ... UPS or other device has an ap9606 ... ... file for the device the card is ... ... your UPS or device has one of these cards ... Your device may still contain ... Only devices with network support are affected. ... your UPS or device has one of these cards ... ... IS SOME MATERIAL CHANGE IN THE FACTS ... ... BE A SIGNIFICANT CHANGE IN THE FACTS ... ... THE INFORMATION CONTAINED HEREIN HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN AN ACTION FOR CONTRACT , STRICT LIABILITY OR TORT (
How do I troubleshoot email failures on a Network Management Card?
Devices with an embedded ... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... Devices with an embedded Network Management Card 1 include (but ... Devices with an embedded ... ... be caused by one or multiple reasons ... ... between the NMC device and mail server ... : NMC1 devices do not support SMTP (email ... NMC2 devices with NMC v ... , and NMC3 devices should provide detailed ... NMC2 devices with NMC v ... , and NMC3 devices should provide detailed ... NMC2 Devices Only: Why ... ... number can be changed as well. ... , and NMC3 devices , SSL/ ...
Bad Gateway message when launching to HTTPS device on StruxureWare private LAN
1 : Change the device launch settings in StruxureWare to use http instead of https.
Network Management Card (NMC) Password Reset Procedure
Devices with an embedded ... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 - AP9617, ... Devices with an embedded Network Management Card 1 include (but ... Devices with an embedded ... ... NMC1 and NMC2 device (s) ... ... below for your device model in order ... ... cause unwanted erratic device behavior. ... Network Management Card 1 Procedure 1 .) ... Network Management Card 1 -enabled device : Device Most UPS devices with a DB ... ... * Indicates the device uses NMC2 password ... ... Management Card Embedded device .
How to navigate through an Network Air FM unit display
... ” on page 25 to set up ... ... work as a single System. ... Half capacity uses one compressor and half ... ... at which to change the order in ... ... should not be changed . ... compressor (stage 1 ) in a ... event to one of the output ... ... and responds to changes in the state ... Provide a unique name for each ... ... If the state changes , the controller ... ... respond to the change of status for an input in one of the following ... ... and events by changing states to notify outside devices . ... , Expansion Module 1 , or Expansion ...
Changing the Line VRMS (Nominal Line Voltage) on your 208/230vac capable Rack Automatic Transfer Switch (ATS)
Go to 1 - Device Manager menu, 3-ATS Configuration and configure item 8-Line VRMS to 208 Important:
MAC address Vendor ID of Network Management Cards, and other network devices changing
... in the format MM : MM : MM :UU: ... , or Organizationally Unique Identifier) and U represents a unique identifier for that device .


Risultati 1 - 10 di 91

Non trovi quello che cerchi?

Contatta l'assistenza clienti per ricevere informazioni, supporto tecnico, assistenza per i reclami e altro ancora.