Technical FAQs

Ask a Question

INTERNAL: Galaxy VX; What is the Airflow and BTU heat dissipation?

INTERNAL ONLY

Issue:
FSRs and or TSE members are asked for the Airflow and BTU / heat dissipation of the Galaxy VX product.


Product line:
Galaxy VX


Environment:
All models, all serial numbers.


Cause:
Air Flow information is not included in the Technical Specification or Installation documentation. BTU/hr information is present in the Technical Specification and Installation documentation.


Resolution:
This table is the estimated airflow in m^3/hr and CFM for the same four load level (three at 30C and one at 40C) as the heat dissipation (BTU/hr) tables found in the documentation.





 
Was this helpful?
What can we do to improve the information ?